![]() |
MCUXpresso SDK API Reference Manual
Rev 2.14.0
NXP Semiconductors
|
Functions | |
| void | bootloader_user_entry (void *arg) |
| Run the Bootloader API to force into the ISP mode base on the user arg. More... | |
| void bootloader_user_entry | ( | void * | arg | ) |
| arg | Indicates API prototype fields definition. Refer to the above user_app_boot_invoke_option_t structure |